A question in MQX Standard PE component

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A question in MQX Standard PE component

2,978 Views
matherinewang
Contributor III

Hi All,

 

i create a new a Kinetis project using Kinetis SDK1.2 and Processor Expert,  and then i add OS componet, and set OS as MQX Standard.

36712_36712.pngpastedImage_6.png      36714_36714.pngpastedImage_9.png

 

After i set as MQX Standard,  PE will add DbgCs1:fsl_debug_console components automatically into Referenced components file foler, shows below.

36708_36708.pngpastedImage_1.png

Then, i got the isue, it's not allowed.  it was added automatically, but then it says not allowed, how can i fix it?

Labels (1)
0 Kudos
Reply
4 Replies

2,825 Views
rqbh
Contributor III

just remove the debug_console component, for mqx has it's own debug out put

0 Kudos
Reply

2,825 Views
matherinewang
Contributor III

Thanks kevin, remove the debug_console componet can fix the problem, but just want to make sure it's okay to remove it.

0 Kudos
Reply

2,824 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Kevin,

yes-exactly. It could be the problem.

Best Regards,

Iva

0 Kudos
Reply

2,824 Views
ivadorazinova
NXP Employee
NXP Employee

Hello matherine wang,

please, can you upload last pic in bigger size?

It is hard to recognize.

Thank you,

Best Regards,

Iva

0 Kudos
Reply