A question in MQX Standard PE component

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A question in MQX Standard PE component

3,195件の閲覧回数
matherinewang
Contributor III

Hi All,

 

i create a new a Kinetis project using Kinetis SDK1.2 and Processor Expert,  and then i add OS componet, and set OS as MQX Standard.

36712_36712.pngpastedImage_6.png      36714_36714.pngpastedImage_9.png

 

After i set as MQX Standard,  PE will add DbgCs1:fsl_debug_console components automatically into Referenced components file foler, shows below.

36708_36708.pngpastedImage_1.png

Then, i got the isue, it's not allowed.  it was added automatically, but then it says not allowed, how can i fix it?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,042件の閲覧回数
rqbh
Contributor III

just remove the debug_console component, for mqx has it's own debug out put

0 件の賞賛
返信

3,042件の閲覧回数
matherinewang
Contributor III

Thanks kevin, remove the debug_console componet can fix the problem, but just want to make sure it's okay to remove it.

0 件の賞賛
返信

3,041件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Kevin,

yes-exactly. It could be the problem.

Best Regards,

Iva

0 件の賞賛
返信

3,041件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello matherine wang,

please, can you upload last pic in bigger size?

It is hard to recognize.

Thank you,

Best Regards,

Iva

0 件の賞賛
返信