writing value to thredhold register creates hard fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

writing value to thredhold register creates hard fault

1,138 次查看
shabanam
Contributor I

Hi

I am using codewarrior 10.3 in windows my task is to develope touchpad with 12 electrodes.

Im using the processor MK40DX256VLQ10

Each electrode is connected to channel TSI0_ch0, TSI0_ch5....TSI0_ch15...

the problem is when i write a value to threshold_0 register it accepts

but then i write value to other register except Threshold_0 reg it creates hard fault..

its urgent

please help...

regards

shabana

0 项奖励
回复
2 回复数

976 次查看
TICS_Fiona
NXP Employee
NXP Employee

CW10.3 is an old verison, could you please update to CW10.5? It can be downloaded from:

http://tinyurl.com/6jo5tge

0 项奖励
回复

976 次查看
shabanam
Contributor I

Hi,

I have also tried CW10.5 and used the latest TSS library(TSS 3.1.0).. still the problem is not solved.

0 项奖励
回复