writing value to thredhold register creates hard fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

writing value to thredhold register creates hard fault

1,088 Views
shabanam
Contributor I

Hi

I am using codewarrior 10.3 in windows my task is to develope touchpad with 12 electrodes.

Im using the processor MK40DX256VLQ10

Each electrode is connected to channel TSI0_ch0, TSI0_ch5....TSI0_ch15...

the problem is when i write a value to threshold_0 register it accepts

but then i write value to other register except Threshold_0 reg it creates hard fault..

its urgent

please help...

regards

shabana

0 Kudos
Reply
2 Replies

926 Views
TICS_Fiona
NXP Employee
NXP Employee

CW10.3 is an old verison, could you please update to CW10.5? It can be downloaded from:

http://tinyurl.com/6jo5tge

0 Kudos
Reply

926 Views
shabanam
Contributor I

Hi,

I have also tried CW10.5 and used the latest TSS library(TSS 3.1.0).. still the problem is not solved.

0 Kudos
Reply