windows usb device disconnect reconnect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

windows usb device disconnect reconnect

跳至解决方案
2,027 次查看
Keith4DSmith
Contributor V

I am using a Kinetis Freedom K22F evaluation board. I have a program running that enables a USB CDC VCOM device.

Windows sees the device just fine and communication is not a problem.

The problem I am having is each time I restart the debug session (I am using Segger J-Trace), I have to physically unplug and replug the USB CDC VCOM cable so I can talk to the device again.

I am using either PuTTY and RealTerm to communicate with the device.

Is there some 'reset' register or reset sequence available with the K22F eval board that one can use to 'simulate' the disconnect and reconnection of the USB device?

标签 (1)
0 项奖励
回复
1 解答
1,803 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Keith,

Thanks for providing more information. I was able to reproduce the behavior you mentioned using Windows7, the example dev_cdc_vcom_bm of the SDK v2.41 and Tera Term.

Please refer to the readme file about this behavior:

<MCUXpresso_SDK_Install>/boards/<board>/usb_examples/usb_device_cdc_vcom_lite/<rtos>/readme.pdf

Since there is no dynamic detection between host and device, the COM port must be closed from the terminal tool prior to plug-out/reset the CDC device. Or the CDC device won't get recognized next time you plug-in with the COM port still opened.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,803 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Keith,

I'm making tests on my side to reproduce this behavior. Could you please tell me which version of Windows are you running? 

Regards,

Victor. 

0 项奖励
回复
1,803 次查看
Keith4DSmith
Contributor V

Windows 7 Enterprise Service Pack 1

Details of usbser.sys at attached in jpgusbser.sys.jpg

0 项奖励
回复
1,804 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Keith,

Thanks for providing more information. I was able to reproduce the behavior you mentioned using Windows7, the example dev_cdc_vcom_bm of the SDK v2.41 and Tera Term.

Please refer to the readme file about this behavior:

<MCUXpresso_SDK_Install>/boards/<board>/usb_examples/usb_device_cdc_vcom_lite/<rtos>/readme.pdf

Since there is no dynamic detection between host and device, the COM port must be closed from the terminal tool prior to plug-out/reset the CDC device. Or the CDC device won't get recognized next time you plug-in with the COM port still opened.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复