use VLPS and pdb-adc?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use VLPS and pdb-adc?

1,716 Views
michaelmac
Contributor I

Hi all, 

is there a way to somehow wake the bus clock for the PDB from the LPTMR, from VLPS, at the same time as using LPTMR for the trig-sel? 

for example, i have the 32k xtal driving the LPTMR. This triggers the PDB, which triggers ADC0 A then B. it works ok in run mode, but i want it to work from VLPS.

im using the FRDM-K22 board. 

thanks,

michael. 

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,602 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Michael Maclean 

This is not possible, because PDB timer doesn't work in VLPS. So evean you LPTMR trigger PDB, this will not work in this mode.

pastedImage_1.png

Hope this information help

Best Regards

Jorge Alcala

0 Kudos
Reply