use VLPS and pdb-adc?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use VLPS and pdb-adc?

1,652件の閲覧回数
michaelmac
Contributor I

Hi all, 

is there a way to somehow wake the bus clock for the PDB from the LPTMR, from VLPS, at the same time as using LPTMR for the trig-sel? 

for example, i have the 32k xtal driving the LPTMR. This triggers the PDB, which triggers ADC0 A then B. it works ok in run mode, but i want it to work from VLPS.

im using the FRDM-K22 board. 

thanks,

michael. 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,538件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Michael Maclean 

This is not possible, because PDB timer doesn't work in VLPS. So evean you LPTMR trigger PDB, this will not work in this mode.

pastedImage_1.png

Hope this information help

Best Regards

Jorge Alcala

0 件の賞賛
返信