undefined symbol Error while building Free-scale_USB_Stack_v4.1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

undefined symbol Error while building Free-scale_USB_Stack_v4.1.1

1,483 Views
karthikas
Contributor IV

I am writing USB driver for the MK60N512MD100 MCU unit for USB-device mode, I downloaded USB stack from free scale website and doing build in Kiel V4. But I am getting fallowing error.

I am using  - Free-scale_USB_Stack_v4.1.1

********************************ERROR_LOG************************************

linking...

.\RAM\USB_CDC.axf: Error: L6218E: Undefined symbol asm (referred from main_kinetis.o).

Not enough information to list image symbols.

Finished: 1 information, 0 warning and 1 error messages.

".\RAM\USB_CDC.axf" - 1 Error(s), 0 Warning(s).

Target not created

**************************************************************************************

Can anyone help me in resolving this issue. Thanks in advance.

0 Kudos
Reply
1 Reply

1,341 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

I'd highly recommend you to choose the USB demos which is from the Kinetis SDK, and the most updated USB stack also integrates into the Kinetis SDK.

Regrading to the USB stack 4.1.1, the updates have been halted, as it has none of teams to cover it now.

Please refer to the thread below to install the Kinetis SDK 2.0

How to: install KSDK 2.0
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------