unable to unlock S32K148

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to unlock S32K148

Jump to solution
2,127 Views
ljmljmljm
Contributor II

Download always show error “Could not find core in Coresight setup”

捕获.PNG捕获1.PNG

捕获3.PNG

0 Kudos
Reply
1 Solution
2,098 Views
ljmljmljm
Contributor II

I've found a solution
resolvent
1) If the hardware circuit board supports modification, the VDD of the chip can be connected to On Pin1 of J_link
2) If the hardware circuit board does not support changes, you can also change the Pin1 and Pin2 short circuit of J_link
Special notes
1) The problem of unable to download the code may appear on all MCU, which will prompt that the chip core cannot be found
2) Pin1 and Pin2 have been short circuited in the new version of j-link (for example, v8.3), so the above problems will not occur
3) Recommendation J_ Link to connect with the target board, please connect to RST signal, that is: VDD, VSS, GND, swdio, swclk, RST signal

View solution in original post

0 Kudos
Reply
2 Replies
2,099 Views
ljmljmljm
Contributor II

I've found a solution
resolvent
1) If the hardware circuit board supports modification, the VDD of the chip can be connected to On Pin1 of J_link
2) If the hardware circuit board does not support changes, you can also change the Pin1 and Pin2 short circuit of J_link
Special notes
1) The problem of unable to download the code may appear on all MCU, which will prompt that the chip core cannot be found
2) Pin1 and Pin2 have been short circuited in the new version of j-link (for example, v8.3), so the above problems will not occur
3) Recommendation J_ Link to connect with the target board, please connect to RST signal, that is: VDD, VSS, GND, swdio, swclk, RST signal

0 Kudos
Reply
2,114 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ljmljmljm,

Please refer: S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply