transferring code to new MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

transferring code to new MCU

1,784 Views
haroldvogel
Contributor II

I have existing code and need to use this code on a new MCU.  I would like to transfer the code and the pin mapping, created by the processor expert function, to this new MCU.  It is a new project so where there was one project there will now be two projects.

0 Kudos
Reply
3 Replies

1,682 Views
haroldvogel
Contributor II

The MCU coming from is MKL36Z128VLL4 going to is MKL36Z256VLL4.

Using CodeWarrior with Processor Expert.

Thanks

John Vogel

0 Kudos
Reply

1,682 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi John,

The difference between those chips are Flash and SRAM size.

For customer is using the Processor Expert tool, customer just need to remove the previous Cpu component: MKL36Z128VLL4 and using the updated MKL36Z256VLL4 Cpu component instead and make related configuration.

Customer doesn't need to change another components configuration.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,682 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Could you provide the existing code based MCU part number? And your target MCU part number?

Which IDE software you are using?

Thank you for the attention.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply