Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
Recently I have received a report which said the customers met compiling issue when they imported the an2295sw CW project file and started to build it, the error message is like the following: When I looked into this issue, I found it was mainly due to some asm source file which was dedicated for Keil wrongly included in the CW project , so there would syntax error during compiling, and the linker issue was due to the path of linker file was wrongly defined, fix them would solve most of the compiling. 1. Fix source file issue: deselect the bootloader.asm file. 2. Fix linker file issue: redefine the correct path for linker file There is also an exception when you try to compile with the configuration for K70 120MHz part, it is due to some files can not be opened because the including path are missing: so besides the above changes, you have to add the paths below to solve this issue for Kinetis 120MHz part.    BTW, during debugging, I also found it is not convenient to switch between different configurations because users have to choose the proper header file for different platforms manually, so I add the following changes to support automatic switching platform according to the configuration but just with an exception for Kinetis K-1M 100MHz part, which still have to choose the proper platform manually. Customers who have downloaded an2295sw may directly replace the following files with that I attached in this document, which have included all above changes mentioned. an2295sw\src\Kinetis\CW_10.3\AN2295_Kinetis\.project an2295sw\src\Kinetis\CW_10.3\AN2295_Kinetis\.cproject an2295sw\src\Kinetis\CommonSource\bootloader_cfg.h Hope that helps, Kan
記事全体を表示
Hi All, all presentations were included in this archive file.
記事全体を表示
底层驱动源码,mdk5.0打开。 另有移植好了的ucGUI的源码。
記事全体を表示
  Hello Freedom community users Few weeks before, I produced for the Element14 community a full video review of the FRDM-KL46Z including all the steps to program and debug your first project example. Video has a length of less than 13 min so your evaluation of the Kinetis KL46 should be really quick and easy http://www.element14.com/community/community/designcenter/kinetis_kl2_freedom_board/blog/2014/06/17/frdm-kl46z-full-review-and-getting-started-in-video Enjoy Greg
記事全体を表示
   1.  K60 eDMA 16-channel implementation Local memory containing transfer control descriptors for each of the 16 channels 32-byte TCD stored in local memory for each channel    2.  DMA memory to memory performance In the traditional M2M data movement, performance is best expressed as the peak data transfer rates In most implementations, this transfer rate is limited by the speed of the source and destination address spaces.     3.  eDMA peak transfer rate   4. Performance test         With K60 100MHz (TWR-K60D100M), implement internal SRAM-SRAM eDMA data transfer. If  transfer size setting as 32-bit in TCD Transfer Attributes (DMA_TCD_ATTR), there will has one wait state during each read/write. That's why the DMA performance doesn't up to 200MB/s as the manual stated.       We highly recommend setting DMA transfer size to 16-byte at DMA_TCD_ATTR register, it will much increase the DMA performance.(Get 162MB/s transfer rate with TWR-K60D100M board.) 5.  Testing code attached.
記事全体を表示
ButtonRace O ∆ []   ButtonRace es un juguete simple, un pequeño invento, que permitirá cambiar la vida de los niños que sufren alguna discapacidad. Nuestra creación está diseñada de una manera muy simple que, a su vez, permite a los niños con capacidades diferentes tener el máximo aprovechamiento. En general, nuestro objetivo era desarrollar los reflejos ojo-mano y estimular el aprendizaje de los niños. Esto, sin caer en las terapias actuales, que al ser tan habituales, pueden volverse menos efectivas. En resumen, el juego consiste en que el niño debe presionar el botón correspondiente a la figura que le es mostrada, lo que permitirá que un pequeña estrella avance a través de una pista de forma determinada. El mecanismo funciona a través del uso de una tarjeta Freedom de Freescale. Además, del uso de una serie de LEDS, un servomotor y algunos sensores infrarrojos y de presión. El sistema está diseñado para darle una retroalimentación al infante, para ver si su respuesta fue correcta. Las figuras encienden en color azul en el momento en que el niño debe presionar algún botón. Dependiendo de si la respuesta fue acertada, la misma figura cambia de color a verde o rojo. Dependiendo de si la figura y el botón corresponden, además, un servomotor moverá la estrella por la pista. Después de varias respuestas correctas, la estrella llegará a una meta, donde el sistema se reiniciará automáticamente. Nuestra intención es que este sistema tan simple de aprendizaje para niños, puede ser utilizado para enseñar otras cosas, además de cumplir nuestro objetivo principal.   Original Attachment has been moved to: Buttonrace.odt
記事全体を表示
Coming Soon.
記事全体を表示
This file was uploaded by the AN4652 author, and is changed from the original release. As far as I can see this file is not in the current zip for the appnote as of apr 25 2013
記事全体を表示
Producto dirigido para terapias visuales y motrices. Consiste en una matriz de 6x3 LEDs, una columna verde, una amarilla y una roja. Aleatoria mente, se encenderá un LED que se encuentra hasta arriba, y ese irá bajando por la columna de su color hasta llegar al ultimo. Cuando eso suceda, se deberá presionar el botón del color correspondiente. Si esto se realiza correctamente, se suma un punto, de lo contrario se restan tres y suena un buzzer. Los puntos se despliegan en pantalla. La velocidad del juego se puede controlar con un potenciometro y un motor Servo se mueve dependiendo del puntaje.
記事全体を表示
The KL TSI Library provides the following benefits: • Reduces time to market and development costs. Already available turn-key TSI Library for IH cooker, remote controller applications, etc. • KL TSI is a hardware touch sensing solution, without any additional peripherals, e.g. Timers, GPIO, CPU execution, as a result reduces overall system cost and size. • Enhances reliability by enabling environment adaptive algorithm, eliminating water droplet and stream influence, and filtering electromagnetic interference. • Easy to use, simplifies user interface design. Flexible TSI software library enabling customers to develop an application • FreeMaster1.4 visualizes TSI signal on screen, thus customer can debug and tune touch software simply.
記事全体を表示
Hello, The below attachment is the code for UART with the input data as a character..But i need the input data to be a STRING...Can anyone please post the code for UART with input as a string using MK22D5.
記事全体を表示
El proyecto está basado en Kinetis KL25Z, consiste en utilizar un tapete de 9 “Botones” y un nunchuck para rehabilitación en piernas y o entrenar sus capacidades sicomotrices llevarlo a cabo atravez de programas especiales en PC, bien esto se lleva acabo utilizando la función de HID de Processor Expert, en el caso del nunchuck funciona como mouse y el tapete como teclado, el joystick del nunchuck actúan como el desplazamiento del mouse y los dos botones con los que cuenta actúan como clic derecho e izquierdo y el tapete actúa como las teclas W, A, S, D, (están son configurables) más 5 teclas adicionales, el tapete está formado por sensores de presión que al pisarlos simulan las teclas correspondientes.     BodyPCcontrol Kinetis Challenge México 2013 - YouTube Original Attachment has been moved to: HID-KEYRUG-KL25Z.rar
記事全体を表示
To do: Implement a program that lets the 4 LEDs on the Tower toggle all together using the PIT Interrupt. For easy debugging, let the program run in the RAM. * toggle period 0.5 s, * extract vector table and service routines in 'vector.c. Hint: Use the 'arm_cm4.c and 'arm_cm4.h' from the freescale kinetis homepage, which include access functions for the NVIC. For ease of use, these routines are included in the result file. Result: TWR_K60_PIT0.zip
記事全体を表示
VREF module provide one input pin VREF, this pin can provide reference voltage for both external circuit but also for internal Sigma Delta ADCs, AFE and DAC.  Also it includes trim function in it. In this document, I would like to use my testing to do a linearity analysis. From figure1 and 2, you can find how to make VREF as reference voltage of different analog module. For example, you can find when S1 switches down, S0 closes and S2 select VREF, VREF will be voltage resource of SAR ADC.                                               Figure 1: Voltage reference function configuration                                   Figure 2: Voltage reference module diagramming I do a testing for VREF trim value linear analysis. The process is connecting the voltmeter to VREFH pin, then record measure result for each setting of VREF trim. There will be 64 records for every different setting. Testing chip is MKM34Z256. Please find my testing result from testing data table. From testing result, you can get the formula that y = kx + x0, where k is about 0.005 (5mV) and x0 is about 1.1881, x is trim value.  You can find there is only a little offset from offset curve.                                         Table 1: Trim voltage testing date                                                                 Figure 3: Offset curve
記事全体を表示
Hi, Anybody has sample code for K22 SPI? where shall I get the same? Thank Sarvani
記事全体を表示
Kinetis芯片在量产时有以下事项需要注意: 1. 保证正确的上电时序,VDD应该先于所有其他引脚上电,VDD上电之前RESET引脚不应该出现高电平。 2. 推荐在RESET引脚加10k上拉电阻,并且和编程器的Reset引脚断开。 3. 编程器至MCU的引线越短越好,最好控制在15厘米之内。 4. 所有引脚不能有超过芯片手册规定之最高电平。 5. 保证焊接温度不超过芯片手册规定之最高温度。
記事全体を表示
To do: Implement a program that lets the 4 LEDs on the Tower toggle all together using the PIT Interrupt. This time, let the program run in the Flash. * toggle period 0.5 s * extract vector table and service routines in 'vector.c' * Change the linker command file 'ldscript_flash' * Take care of the 16 Byte security settings from $400-$410 in the Flash. Do not overwrite!!! Hint: Use the 'arm_cm4.c and 'arm_cm4.h' from the freescale kinetis homepage, which include access functions for the NVIC. For ease of use, these routines are included in the result file. Result: TWR_K60_PIT0_Flash.zip
記事全体を表示
http://dorkbotpdx.org/blog/paul/teensy_audio_library_gets_spdif_support Digital optical audio output from kinetis based teensy 3.1
記事全体を表示
You probably have heard of what's new on Kinetis side of the house. YES, talking about KL02, measuring only 1.9mm x 2.0mm. Take a look at the picture in which this powerful ARM based chip gets compared real scale, and being this tiny yet delivers 60 percent more GPIO than the nearest competing MCU. :smileygrin:!!!
記事全体を表示
DFU_PC_demo_source_code.zip
記事全体を表示