tcp/ip documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tcp/ip documentation

1,898 Views
randyseedle
Contributor III

Is there a document that covers top/ip network programming on the frdm-k64?

Labels (1)
0 Kudos
Reply
1 Reply

1,777 Views
mjbcswitzerland
Specialist V

Hi

NXP bundles LWIP with the SDK so you can use the LWIP documentation.

You can also download the open source version of the uTasker project which includes an integrated TCP/IP stack for the FRDM-K64F board and also allows simulation of all TCP/IP operation for faster learning (this included also integration of FTP/HTTP with file system on SD card or internal memory and TCP/IP operation via the K64 USB port and RNDIS).

Various documents and tutorials about networking: http://www.utasker.com/docs/documentation.html
http://www.utasker.com/forum/index.php?topic=25.0
Various binaries that can be run on the FRDM-K64F or built from the open source project: http://www.utasker.com/kinetis/FRDM-K64F.html
Video showing MQTT on FRDM-K64F and FRDM-K66F bards: https://www.youtube.com/watch?v=-_CV2aXHyjw&list=PLWKlVb_MqDQFZAulrUywU30v869JBYi9Q&index=24


Regards

Mark

Complete Kinetis solutions for professional needs, training and support: http://www.utasker.com/kinetis.html
Kinetis K64:
- http://www.utasker.com/kinetis/FRDM-K64F.html
- http://www.utasker.com/kinetis/TWR-K64F120M.html
- http://www.utasker.com/kinetis/TEENSY_3.5.html
- http://www.utasker.com/kinetis/Hexiwear-K64F.html


uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market
Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis

0 Kudos
Reply