target initiallization failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

target initiallization failed

1,313 Views
hemanth_kl
Contributor I

Hi

We are using Codewarrior 10.6 trial version. We have a board with "MK61FN1M0VMJ12" microcontroller. There is a problem while programming with Universal Mutilink 2.0. 

The error while launching Internal flash configuration is as follows:

___________________________________________________________

fl::target -lc "LC for Simple Flash"
fl::target -b 0x1fff0000 0x20000
fl::target -v off -l off
cmdwin::fl::device -d "FTFE_PFlash1M0" -o "128Kx64x1" -a 0x0 0xfffff
cmdwin::fl::image -f "E:\\CW_WORKSPACE\\DCC_03082017_bel demo final\\MK70FN1M0_INTERNAL_FLASH\\Aslesha_Card_Test.afx" -t "Auto Detect" -re on -r 0x0 0xfffff -oe off
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
Auto-detection is successful.
File is of type Elf Format.

Performing target initialization ...
Error: Connect Failed.
Can't connect. The Debugger can not connect to the P&E device(ARM GDI Protocol Adapter)
Error: Connect Failed.

____________________________________________________________________________________

Earlier, we have tried to do the same process with CW 11, 10.7 versions also but no success could be achieved. We encountered the same error. 

PLEASE REPLY ASAP.

WE ARE STUCK WITH THIS ERROR IN MIDDLE OF A PROJECT. 

Regards

Hemanth K

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,246 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hemanth K,

How about programming a simple project ? And can it debug well using the debugger ?

If still can't work , please check debug configration and flash program configurations:

pastedImage_1.png

BR

Alice

0 Kudos
Reply