speed up Flash execution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

speed up Flash execution

跳至解决方案
2,851 次查看
UB39
Contributor I

Hello!

 

I ve a very perfomance criticle application. So I have to speed up my code. Performance  measurements show that there s a big difference if I boot from Flash or from RAM.  Unfortunately I can only boot from RAM during debugging. It seems that the difference between  RAm and Flashh execution fluctuates very much. I ve code fragments with nearly no difference and some with a 50 percent add on if I boot from flash.

 

So I m very interested why there s such a big fluctuation and how I can reduce the add on for Flash execution.

 

Nearly all of my time critical code is part of a big loop. So maybe it might be a solution to copy the time critical code from Flash to RAM. But how?

 

I use CW 10.1 and a K60N512 Tower Module

 

Many thanks

 

 

 

 

 

0 项奖励
回复
1 解答
2,614 次查看
BenGartner
Contributor II

This appnote describes the process for relocating code to RAM using the linker for Coldfire architecture. The theory is the same for Kinetis. Hopefully this will give you a starting point.

 

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4329.pdf

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,615 次查看
BenGartner
Contributor II

This appnote describes the process for relocating code to RAM using the linker for Coldfire architecture. The theory is the same for Kinetis. Hopefully this will give you a starting point.

 

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4329.pdf

0 项奖励
回复
2,614 次查看
UB39
Contributor I

Thank you very much for the application note. It helps to reduce the overhead for my most time criticle section from 50 percent to around 30 percent. But there s still an overhead between FLASH and RAM booting although I can see in the *.xMAP file that the relocating works fine. 

 

Do you ve got any ideas for the reason?

 

 

0 项奖励
回复
2,614 次查看
UB39
Contributor I

Problem solved.

 

Many thanks

0 项奖励
回复