security flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

security flash

1,632 Views
wulinweng
Contributor II

Dear Support:

I used K64F120M cpu and now we have a function to security the flash, when the flash is security, when do the IN SYSTEM PROGRAM, we should unsecurity the flash.

Do you have any demo source about the K64F120M cpu security and unsecurity?

Thanks & BR,

Mike

Labels (1)
0 Kudos
Reply
1 Reply

1,468 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

The Standard Software Driver (SSD) for C90TFS/FTFx flash provides driver function to preform the unsecure flash operation, and you can download the driver through the link as below.

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fromsite=zh-Hans

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply