security flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

security flash

1,629件の閲覧回数
wulinweng
Contributor II

Dear Support:

I used K64F120M cpu and now we have a function to security the flash, when the flash is security, when do the IN SYSTEM PROGRAM, we should unsecurity the flash.

Do you have any demo source about the K64F120M cpu security and unsecurity?

Thanks & BR,

Mike

ラベル(1)
0 件の賞賛
返信
1 返信

1,465件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

The Standard Software Driver (SSD) for C90TFS/FTFx flash provides driver function to preform the unsecure flash operation, and you can download the driver through the link as below.

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fromsite=zh-Hans

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信