sd card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sd card

1,536件の閲覧回数
chobin
Contributor III

Hello,

I'm working with kinetis k60 and I'm develomping an application that uses an sd card by spi. I check the sd card presence, but I'd like evalute if sd card is working  correctly or Not. I want to do this because sometimes when I turn on the device, the sd card is locked and it is impossibile to comunicate with it unti I cut its power supply. Does someone help  me?

Many  thanks in advance for your support.

Best regards,

Stefano

ラベル(1)
0 件の賞賛
返信
1 返信

1,434件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

K60 product provides ESDHC interface could using to connect with SDCARD, while customer also could using SPI to connect SDCARD.

We have SPI SDCARD example demo based on MQX RTOS, which could be downloaded from here (the latest version is V4.2).

Customer could find TWR-K21D50M board sdcard demo is using SPI mode, the related software could be found at below folder:

C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard\build\iar\mfs_sdcard_twrk21d50m

In the <twrk21d50m.h> file of BSP project, which using SPI1 as SDCARD interface:

/*-----------------------------------------------------------------------------

**                      SDCARD

*/

#define BSP_SDCARD_SPI_CHANNEL           "spi1:"

#define BSP_SDCARD_GPIO_DETECT           (GPIO_PORT_C | GPIO_PIN5)

#define BSP_SDCARD_GPIO_PROTECT          (GPIO_PORT_A | GPIO_PIN17)

#define BSP_SDCARD_DETECT_MUX_GPIO       (LWGPIO_MUX_C5_GPIO)

#define BSP_SDCARD_PROTECT_MUX_GPIO      (LWGPIO_MUX_A17_GPIO)

#define BSP_SDCARD_SPI_CS                (1)

Customer can refer this demo software.

The TWR-K21D50M board related resource could be found at here.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信