saving data on KL43Z in ROM or FLASH during runtime

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

saving data on KL43Z in ROM or FLASH during runtime

ソリューションへジャンプ
3,015件の閲覧回数
thiagopalmieri
Contributor III

Hello,

I have a project that need to persist some data (1 or 2 bytes) during restarts/reboots/resets. It is a configuration information that can be changed during runtime by the user.

Is it possible to share the booitloader ROM space for that or use the flash?

If so, is there any application note or example code that I can look at?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,742件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please download C90TFS_FLASH_DRIVER(TFS Flash Driver Software for Kinetis and ColdFire+ MicroControllers) from here, which includes the KL46 product Flash erase/program operation (customer could refer to storage some data to Flash memory).

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,743件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please download C90TFS_FLASH_DRIVER(TFS Flash Driver Software for Kinetis and ColdFire+ MicroControllers) from here, which includes the KL46 product Flash erase/program operation (customer could refer to storage some data to Flash memory).

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,742件の閲覧回数
thiagopalmieri
Contributor III

Just one last question, how do I read back the data stored ??

Do I use FlashReadResource ??

0 件の賞賛
返信
2,742件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Read data from Flash memory just like read a data from a dedicated address, please refer below code as an example:

//from flash address 0x1000, read 16 bytes back

destination = 0x1000;  // flash address 0x1000

#define BUFFER_SIZE_BYTE          0x10

UINT32 programvalue[BUFFER_SIZE_BYTE];

                for (i = 0; i<BUFFER_SIZE_BYTE; i=i+4)

                {

                    programvalue[i] = *((UINT32 *)(destination+i)) ;

                    printf("\n programvalue[%d] = 0x%4x \n", i, programvalue[i]);

                }

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,742件の閲覧回数
thiagopalmieri
Contributor III

Hello Hui_Ma,

Thank you very much.... I have tried your driver and it works great !!

Regards,

Thiago

0 件の賞賛
返信
2,742件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Any Flash sector can be used to save updateable parameters to (as long as the same sector is not used for code).

See http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF

See also µTasker FRDM-KL43Z support - parameters can be modified and saved to Flash using the command line menu.In the "I/O menu" flash reads, writes and deletes can be experimented with.

Regards

Mark

Kinetis: µTasker Kinetis support

KL43: µTasker FRDM-KL43Z support  / µTasker TWR-KL43Z48M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信