regarding high side switches with KEA128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

regarding high side switches with KEA128

跳至解决方案
1,578 次查看
jashanm
Contributor III

hi all,

       i am working with KEA128 and high side switch (MC07XS6517ET) interfaced via SPI, can i use the 5th and 6th output ? and how can it be used ??

Regards,

Jashan

标签 (1)
0 项奖励
回复
1 解答
1,495 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Jashan

Do you mean that you want to confirm if you can use OUT5 and OUT6 on 07XS6517?

Yes, you can use it. These two pins are not conflict with SPI.

For output control, it is controlled by SPI. You can find from chapter 6.1.2.1 SPI Control and Configuration in datasheet.

http://cache.freescale.com/files/analog/doc/data_sheet/MC07XS6517.pdf

Hope my reply can help you.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,496 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Jashan

Do you mean that you want to confirm if you can use OUT5 and OUT6 on 07XS6517?

Yes, you can use it. These two pins are not conflict with SPI.

For output control, it is controlled by SPI. You can find from chapter 6.1.2.1 SPI Control and Configuration in datasheet.

http://cache.freescale.com/files/analog/doc/data_sheet/MC07XS6517.pdf

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复