regarding high side switches with KEA128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

regarding high side switches with KEA128

ソリューションへジャンプ
1,545件の閲覧回数
jashanm
Contributor III

hi all,

       i am working with KEA128 and high side switch (MC07XS6517ET) interfaced via SPI, can i use the 5th and 6th output ? and how can it be used ??

Regards,

Jashan

ラベル(1)
0 件の賞賛
返信
1 解決策
1,462件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Jashan

Do you mean that you want to confirm if you can use OUT5 and OUT6 on 07XS6517?

Yes, you can use it. These two pins are not conflict with SPI.

For output control, it is controlled by SPI. You can find from chapter 6.1.2.1 SPI Control and Configuration in datasheet.

http://cache.freescale.com/files/analog/doc/data_sheet/MC07XS6517.pdf

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,463件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Jashan

Do you mean that you want to confirm if you can use OUT5 and OUT6 on 07XS6517?

Yes, you can use it. These two pins are not conflict with SPI.

For output control, it is controlled by SPI. You can find from chapter 6.1.2.1 SPI Control and Configuration in datasheet.

http://cache.freescale.com/files/analog/doc/data_sheet/MC07XS6517.pdf

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信