regarding high side switches with KEA128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

regarding high side switches with KEA128

Jump to solution
1,586 Views
jashanm
Contributor III

hi all,

       i am working with KEA128 and high side switch (MC07XS6517ET) interfaced via SPI, can i use the 5th and 6th output ? and how can it be used ??

Regards,

Jashan

Labels (1)
0 Kudos
Reply
1 Solution
1,503 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Jashan

Do you mean that you want to confirm if you can use OUT5 and OUT6 on 07XS6517?

Yes, you can use it. These two pins are not conflict with SPI.

For output control, it is controlled by SPI. You can find from chapter 6.1.2.1 SPI Control and Configuration in datasheet.

http://cache.freescale.com/files/analog/doc/data_sheet/MC07XS6517.pdf

Hope my reply can help you.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
1 Reply
1,504 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Jashan

Do you mean that you want to confirm if you can use OUT5 and OUT6 on 07XS6517?

Yes, you can use it. These two pins are not conflict with SPI.

For output control, it is controlled by SPI. You can find from chapter 6.1.2.1 SPI Control and Configuration in datasheet.

http://cache.freescale.com/files/analog/doc/data_sheet/MC07XS6517.pdf

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply