recovering from VLLS3 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

recovering from VLLS3 problem

ソリューションへジャンプ
2,012件の閲覧回数
namfuak
Contributor III
My target is K60 mask 1N30D. I am developing an application that spends most of the time waiting for external event. While waiting for event the micro should be put in VLLS3 and when wakened up the application must continue from the same point where it was put to sleep. The VLLS3 wakeup goes through a reset so I do the following: save all the relevant registers (i.e. CPU, NVIC, peripheral registers etc) to RAM, configure VLLS3 and perform WFI instruction. On reset I recognize LLWU wakeup, switch to alternate stack, restore all the saved registers, restore saved stack pointer and branch to the instruction next to WFI. Everything works fine. The problem comes I am trying to integrate this stuff to OS scheduler, i.e. when the scheduler can’t find any task able to run, it should put the micro to sleep. The problem is that the scheduler runs in PendSV ISR context. If I branch back to ISR code and load EXC_RETURN value to PC, the CPU tries to fetch instruction from address 0xfffffff9 instead of performing exception return sequence. Ok, so I figured out that in order to return from exception I need to enter to exception first, so when I detect LLWU wakeup, the PendSV is activated, everything is restored, the code jumps to instruction next to WFI and finally does POP PC (LR was pushed to stack at the ISR beginning). Now I am getting usage fault with INVPC bit set… The stack looks just right including LR, PC and XPSR values. I went over “Integrity checks on exception return” chapter in ARM v7m reference manual, all conditions seems to be satisfied and I am stuck. Does anyone tried to do something similar? Any thoughts and advices will be greatly appreciated.
0 件の賞賛
返信
1 解決策
1,786件の閲覧回数
namfuak
Contributor III
The problem is solved: when restoring SCB registers in PendSV ISR context I didn't restored PENDSVACT, as I didn't considered it as part of configuration, so in fact the bit was cleaned. It caused violation of the following rule of integrity check on return from PendSV ISR: "The Exception number being returned from, as held in the IPSR at the start of the return, is listed in the SCB as being active"

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,787件の閲覧回数
namfuak
Contributor III
The problem is solved: when restoring SCB registers in PendSV ISR context I didn't restored PENDSVACT, as I didn't considered it as part of configuration, so in fact the bit was cleaned. It caused violation of the following rule of integrity check on return from PendSV ISR: "The Exception number being returned from, as held in the IPSR at the start of the return, is listed in the SCB as being active"
0 件の賞賛
返信
1,786件の閲覧回数
danielchai
Senior Contributor I

Hi Michael,

When you use OS, how did you implement  LLWU reset part?

Thank you.

-Daniel

0 件の賞賛
返信