project creation in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

project creation in KDS

1,448 Views
snehalnigudkar
Contributor I

Hello,

I have installed Kinetics Design Studio Ver 3.0 & corresponding SDK (ksdk 1.2 update).Now when trying to create new 

project following error appears

pastedImage_3.png

0 Kudos
Reply
2 Replies

1,405 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Snehal,

- If you want use KSDKv1.2, please choose "Kinetis SDK1.X Project" when create project :

pastedImage_1.png

- If you want to use KSDKv2.x, please download the SDKv2.x package as Erich Styger said.

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,405 Views
BlackNight
NXP Employee
NXP Employee

You have to build  and download the SDK for your device from Welcome to MCUXpresso | MCUXpresso Config Tools , it seems you don't have done that?

0 Kudos
Reply