programming kw40z by jlink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

programming kw40z by jlink

3,151件の閲覧回数
shinezen
Contributor III

hello:

i programming kw40z board by jlink (IAR).

the error message ( failed to get cpu status after 4 retries retry ) appear  final step go .

how can i do to solve this problem?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,927件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi,

looks as issue with power supply of MCU. Also you can check if the correct debug connection is selected in IAR (SWD or J-LINK) for Cortex M0+ base MCU has to be SWD.

What kind of debug interface are you using external or integrated in the board for example on freedom board ?

Best regard,

Pavel

0 件の賞賛
返信

2,927件の閲覧回数
shinezen
Contributor III

HI Pavel :

My MCU power from power supplier.

i think i have been programming it but i don't know why i reset power ,the kw40z return initial step .

thanks for you help

圖片4.jpg

圖片2.jpg

圖片3.jpg

0 件の賞賛
返信

2,927件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi,

are you able to do the some steps in the code ? If yes you can check what should be the source of reset. 

Regards,

Pavel

0 件の賞賛
返信