ping_demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ping_demo

1,648件の閲覧回数
maheshwarreddy
Contributor I

hi,

iam using the ping demo application in k66 from sdk2.0 but i can able to send the data which is available at output of the processor but iam not able to see the data in wireshark. if i make the phy loopback the tx data and enable signals are same, what is the problem iam not getting can help us.

0 件の賞賛
返信
1 返信

1,538件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I also do a  test with FRDM-K66F board and lwip_ping_bm demo, with below test result:

pastedImage_1.png

The FRDM-K66F board could get response from PC( IP address: 192.168.1.100).


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信