mke04z128 spi message receiving problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mke04z128 spi message receiving problem

963件の閲覧回数
teknolojiekibic
Contributor I

I am using mke04z128 and mke04z64 for different projects. I am driving ft810 graphic controller via SPI. mke04z64 spi module is working and messages are coming but mke04z128 spi module is not working with same code and same spi configiration. Messages are not coming. I am using codewarrion and processorexpert. what are your recommendations in this regard.

タグ(1)
0 件の賞賛
返信
1 返信

928件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hüseyin Demir,

    Thanks for your interest in NXP kinetis product, I would like to provide service for you.

    As I know mke04z128 and mke04z64 have the same SPI IP. Do you try to run the mke04z64 project in your mke04z128 directly, whether it works or not?

   Please also let me know your chip maskset number, is it the same on the both chip?

   BTW, in your mke04z128 SPI, when the problem happens, do you test the SPI wave, is the SPI bus wave correct or not?  In the CW project, please also disable the code optimization, then try it again, any updated information?

  Any updated information, please kindly let me know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信