mke04z128 spi message receiving problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mke04z128 spi message receiving problem

1,034 Views
teknolojiekibic
Contributor I

I am using mke04z128 and mke04z64 for different projects. I am driving ft810 graphic controller via SPI. mke04z64 spi module is working and messages are coming but mke04z128 spi module is not working with same code and same spi configiration. Messages are not coming. I am using codewarrion and processorexpert. what are your recommendations in this regard.

Tags (1)
0 Kudos
Reply
1 Reply

999 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hüseyin Demir,

    Thanks for your interest in NXP kinetis product, I would like to provide service for you.

    As I know mke04z128 and mke04z64 have the same SPI IP. Do you try to run the mke04z64 project in your mke04z128 directly, whether it works or not?

   Please also let me know your chip maskset number, is it the same on the both chip?

   BTW, in your mke04z128 SPI, when the problem happens, do you test the SPI wave, is the SPI bus wave correct or not?  In the CW project, please also disable the code optimization, then try it again, any updated information?

  Any updated information, please kindly let me know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply