mk60 SWD Pull up resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mk60 SWD Pull up resistor

1,944 Views
ilginsarican
Contributor II

Hello,

I use MK60DN512VLL10 .

Do I have to use pull-up or pull-down resistors for SWCLK and SWDIO lines?

0 Kudos
Reply
3 Replies

1,836 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

No.

These pins have weak internal pull resistors, but external 4.7 kΩ to 10 kΩ pull resistors is recommended.

Debug port pins.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,836 Views
ilginsarican
Contributor II

But is this information valid for K60 Sub-Family?

0 Kudos
Reply

1,836 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes

You can find this table in it's Reference Manual K60P100M100SF2V2RM.

Best Regards,

Robin

0 Kudos
Reply