mbedTLS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mbedTLS

2,738 次查看
fredfu
NXP Employee
NXP Employee

Hi,

    My customer want to use K81 in simple POS project, they need to place SSL in k81, we provided lwip_httpssrv_mbedTLS solution to them. Now there is a issue in authentication, it will be failure if set to server and enable bidirectional authentication, but it is success if set to server and enable unilateralism authentication, it is failure too if set to client and enable bidirectional authentication or unilateralism authentication. Could you help to check? Thanks.

标签 (1)
0 项奖励
回复
2 回复数

2,335 次查看
fredfu
NXP Employee
NXP Employee

Hi,

   We need to modify mbedTLS_buff size from 500 to 2000 in lwip_httpssrv_mbedTLS_freertos.c file. Thanks.

mbedTLS.png

Best Regards,

Fred Fu

0 项奖励
回复

2,335 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanRong,

I am sorry for the delay. I have asked the encryption expert in application team to handle your case, she will give you an answer later.

BR

XiangJun Rong

0 项奖励
回复