mbedTLS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mbedTLS

2,741件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi,

    My customer want to use K81 in simple POS project, they need to place SSL in k81, we provided lwip_httpssrv_mbedTLS solution to them. Now there is a issue in authentication, it will be failure if set to server and enable bidirectional authentication, but it is success if set to server and enable unilateralism authentication, it is failure too if set to client and enable bidirectional authentication or unilateralism authentication. Could you help to check? Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,338件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi,

   We need to modify mbedTLS_buff size from 500 to 2000 in lwip_httpssrv_mbedTLS_freertos.c file. Thanks.

mbedTLS.png

Best Regards,

Fred Fu

0 件の賞賛
返信

2,338件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanRong,

I am sorry for the delay. I have asked the encryption expert in application team to handle your case, she will give you an answer later.

BR

XiangJun Rong

0 件の賞賛
返信