mbed support K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mbed support K70

1,491 Views
kayathrim
Contributor I

Hi,

I have found example project of FRDM-K64 using mbed.It is a ARM cortex M4 core.Will mbed support K70? If yes give details for the same.

Regards,

Kayathri

0 Kudos
Reply
1 Reply

1,292 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello kayathri M:

Currently the Freescale boards supported by mbed are listed in the next link:

Development Platforms with ARM|Freescale

As far as I know there are no plans to support K70. MBED support is created mainly by mbed development team, but community developers can collaborate with the efforts. For details and doubts please visit MBED official website:

mbed | welcome


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------