Over the air firmware upgrade for Kw2x MCUs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Over the air firmware upgrade for Kw2x MCUs.

ソリューションへジャンプ
1,580件の閲覧回数
raheleh
Contributor II

Hello,

Is the following application note applicable to Kw2x series?

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4533.pdf

Thanks!

ラベル(1)
タグ(2)
1 解決策
1,278件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Raheleh Niati:

That appnote applies for Kinetis devices with Flash Swap functionality. Currently there are 4 KW2x devices:

-> KW21D256: Does NOT support Flash Swap

-> KW21D512: Supports Flash Swap

-> KW22D512: Supports Flash Swap

-> KW24D512. Supports Flash Swap

Also, the application note and the code provided (AN4533SW) are useful as reference but the code is not available for KW devices.

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,279件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Raheleh Niati:

That appnote applies for Kinetis devices with Flash Swap functionality. Currently there are 4 KW2x devices:

-> KW21D256: Does NOT support Flash Swap

-> KW21D512: Supports Flash Swap

-> KW22D512: Supports Flash Swap

-> KW24D512. Supports Flash Swap

Also, the application note and the code provided (AN4533SW) are useful as reference but the code is not available for KW devices.

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,278件の閲覧回数
raheleh
Contributor II

Thanks a lot for your reply Jorge!