lpit clock synchronization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpit clock synchronization

1,585 Views
fengning
Contributor I

Hi,

KE1xF Reference manual says:

The timer channels operate on an asynchronous clock,which is independent from the register read/write access clock.Clock synchronization between the clock domains ensures normal operations.

I have two questions:

1.Will the clock synchronization impact  on the ADC or DMA?

2.How long will the clock synchronization take?

Best regards,

Ning

0 Kudos
Reply
2 Replies

1,512 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Ning,

There is a  synchronizer diagram in Figure 41-91(KE1xFP00M168F0RM.pdf). It composed by 2 D flip-flop and has 2 clock source. 

1. I think synchronizer would not impact on ADC or DMA.

2. If the async peripheral clock is slow than bus clock, it will take over 1 async clock to read back.

Regards,

Jing

0 Kudos
Reply

1,512 Views
fengning
Contributor I

Hi Jing,

      Thanks.

      I have a PDB->ADC->DMA module, it works well.

      But if there is a LPIT periodic interrupt, PDB sequence error will happen.

      The PDB as ADC hardware trigger, triggers ADC conversion periodically.

      PDB's interval is a bit longer than ADC conversion time.

      After some test, it seems that LPIT can impact the PDB->ADC->DMA module.

      If i disenable the LPIT interrupt, the module works well.

     So i have doubt that LPIT clock synchronization will block ADC or DMA.

     Or Maybe during LPIT clock synchronization, DMA can't access the bus.

     Thanks again.

 

Regards,

Ning

0 Kudos
Reply