looking for compatible microcontroller.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

looking for compatible microcontroller.

跳至解决方案
2,929 次查看
sudhanshumehta
Contributor IV

Hello All,

We are using MK70FN1M0VMJ15 controller in production and due to chip shortage it is not available.

I have checked with prototype board and MK70FN1M0VMJ12 controller can be used with lesser clock values. It worked with production code made for MK70FN1M0VMJ15. 

Above 2 controllers have 1MB flash.

Now can we use MK70FX512VMJ15 and MK70FX512VMJ12 in place of above 2

These controllers have same pinout and physical size.

Difference between first 2 and later 2 is, first 2 have 1MB flash and later controllers have 512 KB Flash and 512 KB flexMem 

Can my existing software made for MK70FN1M0VMJ15  run on these 512 variants?

 

 

Thanks

Sudhanshu Mehta

 

 

0 项奖励
回复
1 解答
2,878 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport
0 项奖励
回复
3 回复数
2,912 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sudhanshu Mehta,

Yes, If you are sure the original code memory address is not out of range. In addition to the differences you mentioned, you also need to pay attention to the differences in Mask Set (errata).

MK70 difference.pngMK70 difference.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,902 次查看
sudhanshumehta
Contributor IV

Hello Robin,

 

Thanks for your answer. Just for my clarification, you mean we can use MK70FX512VMJ15 in place of MK70FN1M0VMJ15.

just for info, in MK70FN1M0VMJ15  part we have consumed around 990KB flash. 

 

If you are saying yes, this mean 1M flash is 100% equivalent to 512K flash + 512K flex memory.

 

Thanks 

Suddhanshu

0 项奖励
回复
2,879 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for my delay!
Please refer: Programming KW36 FlexNVM with MCUXpresso IDE Example

0 项奖励
回复