linker, bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linker, bootloader

5,644件の閲覧回数
niket_zope
Contributor III

Hello Everyone ! I am a hobbyist.

I am new to linker script modification, (merely focusing on .icf file generated by IAR).

working on development board. MKE1xZ256VLH7.

my requirement are:

I need to create separate sections

1. for Bootloader with 4KB read & exec (best possible to keep where reset vector resides)

2. application code (left space) as read only  in ROM

@mjbcswitzerland can you help ?

Can any one check my changes & provide feedback please !

Attaching my linker modifications.

0 件の賞賛
返信
4 返答(返信)

5,604件の閲覧回数
mjbcswitzerland
Specialist V

Hi

https://www.utasker.com/kinetis/FRDM-KE15Z.html

You can get proven, out-of-the-box boot loaders for most kinetis parts from the uTasker open source project on GitHub: https://github.com/uTasker/uTasker-Kinetis

This contains IAR projects containing linker script files for building the loader and linker scripts for building applications to be loaded that can be used as reference if you prefer to develop a new loader, or as reference for building foreign applications.

Regards

Mark

 


[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements

For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1064.html

0 件の賞賛
返信

5,628件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

If you develop the bootloader, you needn't change the icf. If you develop the application, then you need to change the icf. You can refer this link. It has the icf modification.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

5,619件の閲覧回数
niket_zope
Contributor III

@nxf56274  I don't see any link. Can you share again.

0 件の賞賛
返信

5,613件の閲覧回数
nxf56274
NXP Employee
NXP Employee