l293d connection with frdm k64f

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

l293d connection with frdm k64f

906件の閲覧回数
mymachines88
Contributor I

what are the connection for l293d with FRDM k64f. 

0 件の賞賛
返信
1 返信

853件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mayur Waghela,

   At first, you need to read the L293D datasheet, normally the datasheet have the recommend application :

http://www.ti.com/lit/ds/symlink/l293.pdf 

pastedImage_2.png

Then you if you want to use the K64 to control the L293d, you also need to check the L293d input pin whether can support 3.3V, as you know, the K64 pin output is 3.3V.

  If the 3.3V is not enough, you need to add the circuit to transfer 3.3V to 5V to control L293D.

I find on the web, there have an application contains KL25 and L293D, it may useful to you:

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 1: Servos | MCU on Eclipse 

Wish it helps you!

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信