kv11 flexcan network example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kv11 flexcan network example

1,730 Views
jasonhaedt
Contributor II

Hello I am using the KV11 device and KSDK 1.3.  I noticed there is no flexcan network example.  There was a version started in standalone 1.2 but it did not compile.  Is Freescale working on something that they are able to share for demonstrating the flexcan interface on the KV11 device?

Thank you,

Jason Haedt

Tags (3)
0 Kudos
Reply
1 Reply

1,503 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Jason,

Unfortunately, i have not the example code for FlexCan based on Kinetis, but the MC56F84xxx and Kinetis use the same FlexCAN module, I attach the example based on MC56F84xxx, so that you can refer to it.

BR

Xiangjun Rong

0 Kudos
Reply