kinetis k70 Micro/OS-II

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kinetis k70 Micro/OS-II

1,958件の閲覧回数
gaetanoanania
Contributor III

Hi All,

I have to port the Micro/OS-II into kinetis k70. I read on website of micrium(Micro/OS-II's owner) that there is already the porting ( it can be downloaded) for kinetis k60. My question is: Are there significant differences between k60 and k70 about this porting?

I don't know if anyone has already had experience about this. 

Thank you

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,758件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

TWR-K60N512 board is using K60 100MHz product silicon1.x; TWR-K70F120M board is using K70 120MHz product.

Kinetis 100MHz is using different silicon platform with Kinetis 120MHz product, there are some modules exist difference, such as MCG (clock) module.

I would recommend customer to refer Kinetis 120MHz baremetal example code below:

KINETIS_120MHZ_SC  : Kinetis 120MHz bare metal sample code.

K70_120: Kinetis K70 Graphic LCD 120/150 MHz MCUs

Wish it helps.

0 件の賞賛
返信

1,758件の閲覧回数
gaetanoanania
Contributor III

HI Hui_Ma,

First of all, thank you for you help.

I know that k60 and k70 are different platforms. My question was about the porting of  Micro OS-II. Do you have any experience about that? Or also same documents( It could be a training or a document that talk about this) that could be useful to my aim ( I have to do the porting of  Micro OS-II into the kinetis k70).

Thank you again.

Best regards.

Gaetano

0 件の賞賛
返信