kinetis L: LPO 1khz error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kinetis L: LPO 1khz error

ソリューションへジャンプ
2,587件の閲覧回数
stefanomanca
Contributor III

Hi, anybody knows what is the error of the 1khz lpo oscillator? If yes, are there any documents?

Thank you

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,428件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Stefano,

Digging some more about this, and found this:

http://www.freescale.com/files/32bit/doc/data_sheet/KL25P80M48SF0.pdf

Page 8, Table 6:

pastedImage_1.png

If I read this correctly, then it says that the possible error indeed is +/- 10%.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,428件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I'm using the LPO 1kHz clock for my low power application with LLS (IoT: FreeRTOS Down to the Micro Amps | MCU on Eclipse), and I typically have an error of about 1%.

Erich

2,428件の閲覧回数
stefanomanca
Contributor III

Thanks Erich, in fact I have a 0.8% error but I expect something official from freescale.

0 件の賞賛
返信
2,429件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Stefano,

Digging some more about this, and found this:

http://www.freescale.com/files/32bit/doc/data_sheet/KL25P80M48SF0.pdf

Page 8, Table 6:

pastedImage_1.png

If I read this correctly, then it says that the possible error indeed is +/- 10%.

Erich

0 件の賞賛
返信
2,428件の閲覧回数
stefanomanca
Contributor III

How would I do without you, you're a legend. thank you very much.

0 件の賞賛
返信