kinetis L: LPO 1khz error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetis L: LPO 1khz error

Jump to solution
2,580 Views
stefanomanca
Contributor III

Hi, anybody knows what is the error of the 1khz lpo oscillator? If yes, are there any documents?

Thank you

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,421 Views
BlackNight
NXP Employee
NXP Employee

Hi Stefano,

Digging some more about this, and found this:

http://www.freescale.com/files/32bit/doc/data_sheet/KL25P80M48SF0.pdf

Page 8, Table 6:

pastedImage_1.png

If I read this correctly, then it says that the possible error indeed is +/- 10%.

Erich

View solution in original post

0 Kudos
Reply
4 Replies
2,421 Views
BlackNight
NXP Employee
NXP Employee

I'm using the LPO 1kHz clock for my low power application with LLS (IoT: FreeRTOS Down to the Micro Amps | MCU on Eclipse), and I typically have an error of about 1%.

Erich

2,421 Views
stefanomanca
Contributor III

Thanks Erich, in fact I have a 0.8% error but I expect something official from freescale.

0 Kudos
Reply
2,422 Views
BlackNight
NXP Employee
NXP Employee

Hi Stefano,

Digging some more about this, and found this:

http://www.freescale.com/files/32bit/doc/data_sheet/KL25P80M48SF0.pdf

Page 8, Table 6:

pastedImage_1.png

If I read this correctly, then it says that the possible error indeed is +/- 10%.

Erich

0 Kudos
Reply
2,421 Views
stefanomanca
Contributor III

How would I do without you, you're a legend. thank you very much.

0 Kudos
Reply