kinetis KM35 UART Transmission buffer control of RTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kinetis KM35 UART Transmission buffer control of RTS

ソリューションへジャンプ
3,996件の閲覧回数
jun1
Contributor V

Thank you for all your guidance.

I am using KM35(MKM35Z512VLL7R)
I have a question about the RTS control during UART transmission.

As shown in the figure, the RTS that allows the transmit buffer, when observed on an oscilloscope
It appears to rise one bit before the data to be transmitted.
When transmission is completed, it also appears to fall one bit later.
My questions are the following two points.
(1) Does the time for this one bit change according to the baud rate?
(2) Is there any description of this specification? I looked in the reference manual but could not understand.

Thank you in advance.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,982件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

In order to have in the same channel, Do you read the chapter 45.5.1.7 Transceiver driver enable, from the RM and do not understand?

I review the RM and in the UARTx_MODEM[RXRTSE] the assertion is controlled by this, and this will change depending on the baud rate.

Best regards,
Pavel

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,968件の閲覧回数
jun1
Contributor V

Thank you very much. I understand.

0 件の賞賛
返信
3,983件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

In order to have in the same channel, Do you read the chapter 45.5.1.7 Transceiver driver enable, from the RM and do not understand?

I review the RM and in the UARTx_MODEM[RXRTSE] the assertion is controlled by this, and this will change depending on the baud rate.

Best regards,
Pavel

 

0 件の賞賛
返信