k60 ezport problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k60 ezport problems

1,488件の閲覧回数
lovek61
Contributor I

hi,all,

I am using NXP microcontroller to download bootloader firmware serially(using EZ port) in to K60(MK60DN512ZCAB10R) board .

I am facing following problem:

First,I made reference to the previous diagram which i download from FSL ,there are RCON/RSTI/RSTO pins that can not find in k60,according to the diagram I connect GPIO to k60‘s CS and RESET pin ,but I am not sure about that ,are there anyone can help me  confirm this ?

Second ,according to the previous Demo code ,the sequence for entering Ezport  Mode which I am also not sure about that ,I have already capture the sequence picture in the attachment.The  green line is RESET pin and The yellow line is  CS pin,  are there anybody can help me confirm this ?

kindly  help ~

0 件の賞賛
返信
1 返信

1,155件の閲覧回数
apanecatl
Senior Contributor II

Hi Jack, which schematic/diagram do you refer to?, I don't see any attached files/docs

0 件の賞賛
返信