is there any difference between 'S32 Design Studio IDE' and 'CW V10.6'?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is there any difference between 'S32 Design Studio IDE' and 'CW V10.6'?

ソリューションへジャンプ
2,652件の閲覧回数
taofu
Contributor II

if supported devices quantity is not incorporate, is there any difference between these two IDE?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,204件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello tao

S32DS is:

−Low-cost / No-cost Software Development Tool Strategy

−Low-Cost to develop and maintain

•No-Cost to our customers

•GCC Base Compiler Performance

•Intended to complement and enable Third-Party Partner Tools (Compilers & Debuggers)

•Support for Premium compilers addressing Automotive

Safety Requirements (GHS, Cosmic,...)

•Integration of Freescale software in easy to use

environment for application development (AMMCLIB, MCAT... )

IS NOT

•KDS Equivalent

•AUTOSAR software

•CodeWarrior Replacement

•Premium Tool Replacement (w/ Advanced Debugging,

Best in class code performance, etc...)

S32DS is Basic Tool Frame Work which includes:

• GNU C/C++ Compiler (GCC from ARM Cortex-M and A cores,

GCC for Power Architecture, Standard Solid Compilers)

•Basic Eclipse Backplane

•GNU GDB Debugger:  Basic Debugger interface to low cost JTAG debugger

(Pemicro, Segger, and OpenOCD)

CodeWarrior supports multiple architecture (S08,RS08,S12,S12X,S12Z,DSC,Coldfire, PowerPC and Kinetis) . CodeWarrior comes with its own compiler, proprietary ANSI and runtime library, and is using a proprietary debugger engine. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,205件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello tao

S32DS is:

−Low-cost / No-cost Software Development Tool Strategy

−Low-Cost to develop and maintain

•No-Cost to our customers

•GCC Base Compiler Performance

•Intended to complement and enable Third-Party Partner Tools (Compilers & Debuggers)

•Support for Premium compilers addressing Automotive

Safety Requirements (GHS, Cosmic,...)

•Integration of Freescale software in easy to use

environment for application development (AMMCLIB, MCAT... )

IS NOT

•KDS Equivalent

•AUTOSAR software

•CodeWarrior Replacement

•Premium Tool Replacement (w/ Advanced Debugging,

Best in class code performance, etc...)

S32DS is Basic Tool Frame Work which includes:

• GNU C/C++ Compiler (GCC from ARM Cortex-M and A cores,

GCC for Power Architecture, Standard Solid Compilers)

•Basic Eclipse Backplane

•GNU GDB Debugger:  Basic Debugger interface to low cost JTAG debugger

(Pemicro, Segger, and OpenOCD)

CodeWarrior supports multiple architecture (S08,RS08,S12,S12X,S12Z,DSC,Coldfire, PowerPC and Kinetis) . CodeWarrior comes with its own compiler, proprietary ANSI and runtime library, and is using a proprietary debugger engine. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,204件の閲覧回数
taofu
Contributor II

thank you very much, it is very helpful for me.

0 件の賞賛
返信