is there any difference between 'S32 Design Studio IDE' and 'CW V10.6'?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is there any difference between 'S32 Design Studio IDE' and 'CW V10.6'?

Jump to solution
2,701 Views
taofu
Contributor II

if supported devices quantity is not incorporate, is there any difference between these two IDE?

Labels (1)
0 Kudos
Reply
1 Solution
2,253 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello tao

S32DS is:

−Low-cost / No-cost Software Development Tool Strategy

−Low-Cost to develop and maintain

•No-Cost to our customers

•GCC Base Compiler Performance

•Intended to complement and enable Third-Party Partner Tools (Compilers & Debuggers)

•Support for Premium compilers addressing Automotive

Safety Requirements (GHS, Cosmic,...)

•Integration of Freescale software in easy to use

environment for application development (AMMCLIB, MCAT... )

IS NOT

•KDS Equivalent

•AUTOSAR software

•CodeWarrior Replacement

•Premium Tool Replacement (w/ Advanced Debugging,

Best in class code performance, etc...)

S32DS is Basic Tool Frame Work which includes:

• GNU C/C++ Compiler (GCC from ARM Cortex-M and A cores,

GCC for Power Architecture, Standard Solid Compilers)

•Basic Eclipse Backplane

•GNU GDB Debugger:  Basic Debugger interface to low cost JTAG debugger

(Pemicro, Segger, and OpenOCD)

CodeWarrior supports multiple architecture (S08,RS08,S12,S12X,S12Z,DSC,Coldfire, PowerPC and Kinetis) . CodeWarrior comes with its own compiler, proprietary ANSI and runtime library, and is using a proprietary debugger engine. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,254 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello tao

S32DS is:

−Low-cost / No-cost Software Development Tool Strategy

−Low-Cost to develop and maintain

•No-Cost to our customers

•GCC Base Compiler Performance

•Intended to complement and enable Third-Party Partner Tools (Compilers & Debuggers)

•Support for Premium compilers addressing Automotive

Safety Requirements (GHS, Cosmic,...)

•Integration of Freescale software in easy to use

environment for application development (AMMCLIB, MCAT... )

IS NOT

•KDS Equivalent

•AUTOSAR software

•CodeWarrior Replacement

•Premium Tool Replacement (w/ Advanced Debugging,

Best in class code performance, etc...)

S32DS is Basic Tool Frame Work which includes:

• GNU C/C++ Compiler (GCC from ARM Cortex-M and A cores,

GCC for Power Architecture, Standard Solid Compilers)

•Basic Eclipse Backplane

•GNU GDB Debugger:  Basic Debugger interface to low cost JTAG debugger

(Pemicro, Segger, and OpenOCD)

CodeWarrior supports multiple architecture (S08,RS08,S12,S12X,S12Z,DSC,Coldfire, PowerPC and Kinetis) . CodeWarrior comes with its own compiler, proprietary ANSI and runtime library, and is using a proprietary debugger engine. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,253 Views
taofu
Contributor II

thank you very much, it is very helpful for me.

0 Kudos
Reply