in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

774 次查看
kalpananachneka
Contributor I

in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

标签 (1)
0 项奖励
回复
1 回复

653 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Kalpana,

Definitely, they are independent.

And I'd highly recommend you to refer to the KSDK development kit which provides the several kinds of the demo applications and the demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution and the capabilities of the peripheral drivers.

KSDK:

Software Development Kit for Kinetis MCUs|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复