in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

764 Views
kalpananachneka
Contributor I

in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

Labels (1)
0 Kudos
Reply
1 Reply

643 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Kalpana,

Definitely, they are independent.

And I'd highly recommend you to refer to the KSDK development kit which provides the several kinds of the demo applications and the demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution and the capabilities of the peripheral drivers.

KSDK:

Software Development Kit for Kinetis MCUs|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply