i.mx rt1020 evk board a new project using keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx rt1020 evk board a new project using keil

1,369 Views
bilge_kara157
Contributor II

I started to use i.mx rt1020 evk board and I try to create a new project using keil ,but there is always errors.

How can I create a new project on keil ?Is there any document in this topic?

0 Kudos
Reply
2 Replies

1,193 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi bilge kara,

   Last time, please create your I.MX RT question in the i.mx area:

  i.MX Processors 

   This time, I reply you directly.

   If you want to create the rt1020 keil project, I suggest you refer to the official SDK keil project, which can be downloaded from this link:

   Welcome | MCUXpresso SDK Builder 

  Select the RT1020 processor, generate the code, and download it.

  You can refer to the simple project, eg: SDK_2.5.0_EVK-MIMXRT1020\boards\evkmimxrt1020\demo_apps\led_blinky\mdk

   If you just want to run it from RAM, you can use these files as the startup file:

pastedImage_3.png

  You can totally create a project which is the same as the KSDK, after add the files, in the options, you need to add the include paths:

pastedImage_4.png

Please try it on your side.

Wish it helps you!

If you still have question, you can create the new post in the I.MX area, then I will provide the detail support for you.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,193 Views
mjbcswitzerland
Specialist V

Hi

I think you need the i.MX forum rather than the Kinetis forum.

Regards

Mark

0 Kudos
Reply