i can not debbug in the KL25Z FRDM...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i can not debbug in the KL25Z FRDM...

跳至解决方案
2,709 次查看
josealonsovalle
Contributor III

Hi, I am new in this of the kinetis microcontroller, and i have the FRDM KL25Z but when i wanna debbug, codewarrior shows  a error alert....Can somebody help me please??...

ddd.PNG.png

1 解答
2,320 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jose,

have you switched to the SDA debug application? It looks like you are running the wrong firmware for debugging.

See

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

在原帖中查看解决方案

5 回复数
2,320 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

By default the firmware running in the OpenSDA device is the MSD, you have to program the debug application into OpenSDA.

Follow the OpenSDA User Guide.

http://cache.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf?fpsp=1&WT_TYPE=Users Guides&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

  1. Getting into Bootloader Mode
  2. Program the P&E Debug Application

Then CW will detect your debugger device.

Best Regards,

Luis

2,321 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jose,

have you switched to the SDA debug application? It looks like you are running the wrong firmware for debugging.

See

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

2,320 次查看
josealonsovalle
Contributor III

Thanks bro, already i can debbug my board....

0 项奖励
回复
2,320 次查看
nasreenshaikh
Contributor III

HI Jose,

     Which device are you using for debugging? Multilink, Cyclone pro, Jtag, or OSBDM? you will need the drivers for whichever debugging tool you are using.

0 项奖励
回复
2,320 次查看
josealonsovalle
Contributor III

Hi, i believe that is the OPEN SDA, and i did install the drivers of the FRDM. The KL25 FRDM don't need a BDM..

0 项奖励
回复