how can i read data from a usb device in k70 tower kit(TWRK70120F) and display it in a tft display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i read data from a usb device in k70 tower kit(TWRK70120F) and display it in a tft display

979 Views
sreekanthpk
Contributor I

i need to read  a content from a usb (otg) in twrk70f120m

how can i do it?i also want to display it in the tft lcd display

please help

0 Kudos
Reply
1 Reply

772 Views
isaacavila
NXP Employee
NXP Employee

Hello,

Which USB stack are you using? For example, in BareMetal USB stack 4.1.1, there are some examples for USB OTG functionality and basically, after initializing the USB module and configure it as OTG, you can use Device or Host APIs to send/receive data by calling (depending on current mode):

(Sending data to Host)

USB_Class_HID_Send_Data(CONTROLLER_ID,HID_ENDPOINT,rpt_buf, KEYBOARD_BUFF_SIZE);

or

(Receiving data from Device)

_usb_host_recv_data(host_handle, pipe, &tr);

MQX Classic (MQX 4.2) does also have support for Host or Device and APIs are almost the same. You can consult examples on these stacks.

Hope this helps!

Regards,

Isaac

0 Kudos
Reply