hid multiple endpoints

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hid multiple endpoints

2,711 Views
kamransial
Contributor I

Hi i am trying to make multiple endpoints using the sample code of usb hid mouse mqx k20 but only one endpoint is sending data to pc other endpoint does not initialize. i made 2 interfaces each with one endpoint and used these commands to initialize two different hid devices  

g_mouse2.app_handle = USB_Class_HID_Init(&config_struct2);

g_mouse.app_handle = USB_Class_HID_Init(&config_struct);

Labels (2)
0 Kudos
Reply
1 Reply

1,914 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello,

 

The HID Mouse example of MQX doesn’t include the descriptors for supporting OUT endpoints. It is required to add this support, and modify the Device and Interface descriptors, besides of adding the related Endpoint descriptors. On the following thread you will find an implementation of a Generic HID device based on the bare-metal Freescale USB Stack and a S08JS16 device. The low level implementation is almost the same for MQX and K20, so you could use it as reference:

 

https://community.freescale.com/message/320915#320915

 

Hope this will be useful for you.

Best regards!

/Carlos